Tìm các câu hỏi thường gặp
What is the combination SCCR rating for ATSU01 with the U-Line starters?
Issue:
Customer is using the ATSU01 with the mounted Tesys U-Line motor starter. They are looking to coordinate the short circuit current rating.
Product line:
ATSU01, U-Line, Altistart 01, ATS01
Environment:
All models.
Cause:
n/a
Resolution:
Per Product Marketing, we do not have any combination SCCR ratings for the ATSU01 and U-Line devices. The ATSU01 and ATS01 have a standalone rating of 5kA. Except the ATS01N103FT and ATS01N106FT, which are 1kA.
Customer is using the ATSU01 with the mounted Tesys U-Line motor starter. They are looking to coordinate the short circuit current rating.
Product line:
ATSU01, U-Line, Altistart 01, ATS01
Environment:
All models.
Cause:
n/a
Resolution:
Per Product Marketing, we do not have any combination SCCR ratings for the ATSU01 and U-Line devices. The ATSU01 and ATS01 have a standalone rating of 5kA. Except the ATS01N103FT and ATS01N106FT, which are 1kA.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: