Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
EEM 5.0 - ETL Fails to Extract Data
Issue:
ETL versions 3.0.13325.02 and 3.0.14050.01 produce the following error when attempting to extract data out of EEM.

2014-08-14 08:34:06,007 ERROR ETLEngine (Job_HTML) - Thread ID (4) - EEM Extract Task: Task EEM Extract Task failed
System.ArgumentException: An item with the same key has already been added.
at System.Collections.Generic.Dictionary`2.Insert(TKey key, TValue value, Boolean add)
at SchneiderElectric.ETL.EEM50.EEMExtractTask.DataTableToDictionary(DataTable dt)
at SchneiderElectric.ETL.EEM50.EEMExtractTask.PrepareForExtract()
at SchneiderElectric.ETL.Core.SQThreadExtractTask.Extract(TaskData data)
at SchneiderElectric.ETL.Core.ExtractTask.DoWork()
at SchneiderElectric.ETL.Core.Task.Execute()
2014-08-14 08:34:06,090 ERROR ETLEngine (Job_HTML) - Thread ID (1) - A fatal exception occurred while executing the job.
System.ApplicationException: Task Execution Failed ---> System.ApplicationException: Task EEM Extract Task failed ---> System.ArgumentException: An item with the same key has already been added.
at System.Collections.Generic.Dictionary`2.Insert(TKey key, TValue value, Boolean add)
at SchneiderElectric.ETL.EEM50.EEMExtractTask.DataTableToDictionary(DataTable dt)
at SchneiderElectric.ETL.EEM50.EEMExtractTask.PrepareForExtract()
at SchneiderElectric.ETL.Core.SQThreadExtractTask.Extract(TaskData data)
at SchneiderElectric.ETL.Core.ExtractTask.DoWork()
at SchneiderElectric.ETL.Core.Task.Execute()
--- End of inner exception stack trace ---
--- End of inner exception stack trace ---
at SchneiderElectric.ETL.Core.Job.Execute()
[Job Logger Finished]

Product Line:
ION EEM 5.0

Environment:
ETL versions 3.0.13325.02 and 3.0.14050.01 with ION EEM 5.0

Cause:
There are duplicate source name(s) contained within the database.
The ETL uses the source name as a key in a dictionary to perform the extraction.

Resolution:
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

Execute the following SQL select statement to identify the duplicate source(s) :
SELECT count(Name)as countname, Name FROM SRC_Source group BY Name having count (*) > 1 order by countname
Using Edit Mode in SQL Management Studio, modify the source name(s) identified issuing the following SQL select statement:
Select *  from SRC_Source where Name = "(name to be edited)"
In the results pane returned from the above query, click on the Name column, and edit so that each row contains a unique value.