Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How is a fault code cleared or reset, on ATS22?
Issue:
Needs to clear a fault code, on the ATS22 soft start.

Product Line:
Altistart 22

Environment:
All models

Cause:
The fault code must be cleared to make ATS22 functional.

Resolution:
After the condition that created the fault has been corrected, a fault reset can be accomplished several ways:

1) Remove control power from CL1-CL2. After the display has gone blank, apply control power.
2) On the integral or remote keypad, press the 3-key combination of ENT / UP arrow / DOWN arrow, simultaneously.
3) Wire a reset contact to logic input LI2 or LI3 and program it to rSt (remote reset). A momentary contact closure will reset.
4) Use Modbus command word 752 and write a 1 to bit 3

Note that several fault codes require method 1) above.  These are InF, trAP, SCF.