Issue:
Autotuning on a ATV312 when running multimotors.
Product Line:
ATV312
Environment:
All
Cause:
Installation / Setup
Resolution:
Auto tuning should not be completed when using multiple motors. An Autotune should only be completed when using a single motor. The motor should be cold (typically left to sit over night).
Đã phát hành cho: Schneider Electric Việt Nam