Hôm nay chúng tôi có thể giúp gì cho bạn?

What is the part number of the replacement control board for the ATS48?

Article available in these languages:

  • Tiếng Tây Ban Nha

Issue:
ATS48 control board part number replacement.

Product Line:
Altistart 48

Resolution:
The control board is part number VX4G481, common to all ATS48 model and part numbers.
*Does not work with the newer ATS480 softstarts