Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is there a way to restore the default username and password for the web page access to the Quantum Ethernet module?
Issue
Is there a way to restore the default username and password for the web page access to the Quantum Ethernet modules.

Product Line
140CPU65260, 140NOE77101

Environment
Windows 10 version 1902,

Resolution
The user lost the password and cannot access the web pages in the Quantum Ethernet modules.
They need tp restore the default username and password.

The only way to restore the default username and password is to go into the Quantum Ethernet module to delete a specific file.This requires using an internal proprietary username and password to access it.  Due to security reasons, this username and password cannot be given out to either the customer or a Schneider Electric representative. In order to restore the default username and password, the Quantum Ethernet module will need to be sent back for repair.