Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Changes between Unity 8 and Unity 8.1 for READ_VAR and WRITE_VAR

Issue
Changes between Unity 8.0 and Unity 8.1 for READ_VAR and WRITE_VAR

Product Line
EcoStruxure Control Expert (formerly known as Unity Pro)

Environment
Unity Pro v8.1

Resolution
The 'types Library Manager show that the version has changed in the READ_VAR and WRITE_VAR blocks.  The
online help and release notes do not describe the changes between Unity 8 and Unity 8.1  for the READ_VAR and
WRITE_VAR.

The changes is described below.

'READ_VAR':
Unity V8.0 READ_VAR version V1.01

  • Added support Ethernet Remote IO drops.

Unity V8.1 READ_VAR version V1.02

  • Added the attribute for the new Safety PLC (MC80 or M580)Safety. Only the attribute was modified, no functional changes were added.

'WRITE_VAR':
Unity 8.0 WRITE_VAR version 1.02

  • Added support Ethernet Remote IO drops.

Unity 8.1 WRITE_VAR version 1.03

  • Added the attribute for the new Safety PLC (MC80 or M580). Only the attribute was modified, and no functional changes were added.