Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Cannot delete type 2 user from the Unity Security Editor
Issue
Cannot delete 'Type 2' user from the Unity Security Editor

Product Line
EcoStruxure Control Expert (formerly known as Unity Pro)

Environment
Unity Pro v8.1

Resolution
Exporting the list of users for the Concept security editor creates a text file that shows the user as a 'Type 2'.  If you import the file into the Unity Security Editor, the 'Type 2' user will be added as a predefined user.  If you try to delete the user from the Unity Security Editor, it returns the error message  'user_xxxxx is a predefined user.  Predefined users cannot be deleted or modified.  Delete cancelled.'.  If you try to uninstall the editor by deleting Unity and reinstalling it, the user will still be shown in the list for the Security Editor.

The pre-defined users for Security Ediotr does not get deleted when Unity is uninstalled using the Control Panel.  The only way to delete the user is to uninstall Unity by using the 'UPCleaner.exe' tool for Unity and deleting any Unity installed folder.  Each version of Unity has it's own version of the UPCleaner tool.  To obtain the correct version of the UPCleaner tool, contact your local Schneider Electric help desk.