Issue
ION Setup is showing no decimal precision for either the data recorders or the real time data
Product line
ION Setup
Cause
The regional formatting is set to an non-North American standard for decimal point ( a comma instead of a period) which causes the decimal points to incorrectly be dropped.
Resolution
Upgrade to ION setup V3.0.15233.1 or newer from the link below:
https://www.se.com/ww/en/download/document/ION_Setup_Latest_Release/
Đã phát hành cho: Schneider Electric Việt Nam