Hôm nay chúng tôi có thể giúp gì cho bạn?

ION Setup does not allow user to add new device name that starts with number like "123test"

Issue
ION Setup does not allow user to add new device name that starts with number like "123test". When customer enter their new device name to be "123test" then it does not let them configure the rest of the options such as device type and unit ID.

Product Line
ION Setup 3.0

Cause
Customer would like to name their new device that starts with number. For example, "123test".

Enviornment
Customer would like to name their new device that starts with number. For example, "123test".

Resolution
Some older version of ION Setup had restriction where it didn't allow users to configure device name that starts with numbers.

Customer should upgrade their ION Setup version to 3.0.15233.01 or older in order to resolve this issue. In the latest version of ION Setup, customer can configure their device name that starts with number as shown in picture below:

New Device