Issue:
Is there a remote keypad for the ATS48?
Product Line:
ATS48
Environment:
All
Cause:
Remote keypad required
Resolution:
Part number VW3G48101 is the kit, and includes:
Keypad with 3–character 7–segment display,
IP65 cover and seal,
Mounting screws,
3 meter cable to connect keypad display to Altistart 48.
Note: The kit is not rated for outdoor use.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
Đã phát hành cho: Schneider Electric Việt Nam