Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
When using a USOPTL4 (RS485-USB adapter) in Power Monitoring Expert the serial site times out, however Modbus Tester can successfully connect to the adapter

Issue
Customer has a daisy chain connected serially to the computer using RS485-USB adapter (Model#: USOPTL4). He can connect to any meter on that daisy chain and read registers using Modbus Tester (See FA180037 to learn more about Modbus Tester). However when using the adapter as a serial site in PME, the connection times out.

Product Line
RS485-USB adapter (Model#: USOPTL4)

Environment
ION Enterprise 6.0 SP1
StruxureWare Power Monitoring 7.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Modbus Tester

Resolution
Modbus Tester software requires the "Echo" dip switch (located on the back of RS485-USB adapter) to be ON when communicating with Modbus devices.
Power Monitoring Expert, StruxureWare Power Monitoring, and ION Enterprise require "Echo" to be OFF when communicating with devices.
ION Setup 3.0 configuration software also requires "Echo" to be OFF.
aa