Hôm nay chúng tôi có thể giúp gì cho bạn?

Sepam 10 error code list

Issue

A user is looking for the list of error codes applicable to the Sepam 10 protection relay and requires information regarding the availability and usage of this document.

Product

  • Sepam Series 10

Environment

  • Sepam Series 10 protection relays
  • Troubleshooting and maintenance activities
  • Technical support and diagnostic investigations

Cause

When diagnosing relay behavior or faults, users may need to reference error codes generated by the Sepam 10 device. The error code list is maintained as a technical reference document.

Resolution

The Sepam 10 Error Code List is available in a dedicated reference document containing the error codes and their corresponding descriptions.

Important Notes:

  • The error code list is intended for internal use only.
  • The referenced document is available in French language.
  • When troubleshooting Sepam 10 devices, consult the error code list to identify the meaning of reported errors and support diagnostic activities.

Schneider Electric Việt Nam

Phần đính kèm
Liste des erreurs Vipam.pdf [92.61 KB]