Tìm các câu hỏi thường gặp
Rope pull switches XY2C - Tightening torque values of the XY2CE, XY2CED, XY2CH, XY2CJ mounting screws, not delivered with the rope pull switch
For the rope switch pull enclosure fixing, the concerned XY2C* user instructions or instruction sheets provide the following recommended tightening torques for the fixing screws, not supplied with the product. Applied value depends mainly on the support material.
- XY2CH and XY2CE or XY2CED rope pull switches : screws M6, tightening torque = 4 +/-0.5 N.m (Newton x meter) or 35.4 +/-4.4 lbf.in (pound x inch);
- XY2CJ : screws M5, tightening torque = 3 +/-0.6 N.m (Newton x meter) or 26.55 +/- 5.3 lbf.in (pound x inch).
- XY2CH and XY2CE or XY2CED rope pull switches : screws M6, tightening torque = 4 +/-0.5 N.m (Newton x meter) or 35.4 +/-4.4 lbf.in (pound x inch);
- XY2CJ : screws M5, tightening torque = 3 +/-0.6 N.m (Newton x meter) or 26.55 +/- 5.3 lbf.in (pound x inch).
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Tìm hiểu thêm