Hôm nay chúng tôi có thể giúp gì cho bạn?

Unity Pro and Control-Expert allow to modify the period value, during runtime (in the M580 CPU animation window). Is this value kept after a warm or cold restart?

No, this value is no memorized.
it will be reset to the the configured value when the CPU restarts.