Does Schneider Electric have any Altivar drives that do regeneration?

Issue:
Energy Regeneration on Altivar drives

Product Line:
Altivar Process 980 Regeneration Drive

Resolution:
The Active Front End (AFE), Altivar Process 980 Drive system is a packaged, high-performance solution for regenerative applications. This regenerative drive is highly efficient in four-quadrant technology for speed control in both directions. The horsepower range is 150hp - 900hp.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: