Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
In Vijeo Designer, why does the Panel Action node still remain after I've deleted all the actions inside?
Issue:
The Panel Action Node still appears after we delete all actions associated the panel.

Product Line:
Vijeo Designer (all versions)

Resolution:
The Panel Action node will remain once it has been created in your Vijeo Designer application, even if all actions are deleted in the Panel Action node.

There is no harm in having this panel action remain under each panel where an action has been deleted.