Do the VED kits fit onto the roofs of the Symmetra UPS?
Issue:
A customer may want to add a VED Kit to a Symmetra UPS.

Product Line:
Network Air and Symmetra

Environment:
All versions and serial ranges.

Cause:
A customer may want to provide cooling to a Symmetra that's installed in a row of cabinets by utilizing Vertical Exhaust Duct Kits.

Resolution:
The VED kits are not compatible with the Symmetra roof design.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: