Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to correct the spelling of the Measurement StandardName in EEM through SQL Database Edits
Issue
User has a spelling mistake in a measurement name and wants to correct the name beyond just updating the display name.

Product
ION EEM 3.95 Sp1, 4.0, 4.0R2, 5.0

Environment
SQL Server Management Studio (SSMS)

Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

1) Open SSMS and connect to the EEM database
2) Expand Databases --> ION_EEMData -->Tables
3) Right click on dbo.TS_Resources and select "Edit top 200 rows"
4) Click the "Show SQL Pane" Icon and add the filter "Where Name like '[name of incorrect measurement]' " (without double quotes)
5) Click execute
6) Modify the name to the correct spelling
7) Click on a new line to commit the changes
8) Repeat steps 3 through 7 on tables dbo.RPT_Measurement and dbo.MM_MeasurementMap updating DisplayName, FullName and StandardName