Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How to obtain the nameplate information of a MiCOM relay from its settings file
Issue
User would like to verify/check the serial number, model number, hardware revision and software revision from the MiCOM settings file.

Product Line
MiCOM Relays (All)

Resolution
To view Nameplate info of a Px4x relay:
1- Open the settings file of the relay on Easergy Studio Software by double clicking on it.
2- expand system data as shown below
3- The Model number, serial number and software revision information should be visible.

Image 1

To view Nameplate info of a Px3x Relay:
1- Open the settings file of the relay on Easergy Studio Software by double clicking on it.
2- Expand Device ID and navigate to DVICE as shown below.
3- The DVICE menu will have the following parameters: Device Type, Software version, Serial number and order number.
Image 2