Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
PME 8.0/8.1 - Designer crashes when attempting to open a 3300 ACM meter

Issue
When attempting to open a 3300 ACM in Designer to configure the meter, the system prompts the following error and results in a crash.

ACM Error in Designer

Product Line

330 ACM Meter
Power Monitoring Expert 8.0

Power Monitoring Expert 8.1

Environment
Power Monitoring Expert Designer Application

Cause
Designer crashes as a result of the ACM 3300 meter returning "330" for its Device type rather than "3300".

Resolution
**Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).
A patch is available to resolve this issue within Designer. (set3300.zip attached below)
To deploy this patch, please perform the following:

  • Make a backup copy of set3300.dat, which you will find in the following folder: <PME installation folder>\system\etc
    • E.g. C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\etc\set3300.dat
  • Copy the new version of set3300.dat over top of the original version.

Alternatively, as a workaround you may use ION Setup to perform the meter configuration. (The latest version of ION Setup can be obtained from FA212816)
*It is expected that support for the 3300 in Designer will be phased out in a future software release.

Schneider Electric Việt Nam

Phần đính kèm
set3300.zip [5.53 KB]