Issue:
Needs the total DC bus capacitance for the ATV960 in microfarads
Product Line:
ATV960
Environment:
All
Cause:
N/A
Resolution:
The DC capacitance for the ATV660/960 is 10mF per brick.
1p: ATV960C11 ... C16: 10mF
2p: ATV960C20 ... C31: 20mF
3p: ATV960C35 ... C50: 30mF
4p: ATV960C56 ... C63: 40mF
5p; ATV960C71 ... C80: 50mF
Đã phát hành cho: Schneider Electric Việt Nam