Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
ATV630 Why am I getting Motor Short circuit fault when switching STOA or STOB with an external power supply?
Issue:
ATV630 -getting Motor Short circuit fault when switching STOA or STOB, with an external power supply.

Product Line:
ATV630 process drive.

Environment:
All models and serial numbers with firmware revision below 1.3IE07

Cause:
Firmware issue.

Resolution:
This situation was verified as a problem with the drive firmware and was repaired with firmware release V1.3IE07.  If you have a 630 process drive with firmware below V1.3IE07, upgrading the firmware will correct this problem.