Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can we take the content from a File System Download and convert it back to a VDZ file so that we can make modifications in Vijeo Designer?
Issue:
Looking for a way to take the File System Download content and convert it back to a VDZ file so that we can make modifications in Vijeo Designer.

Product Line:
Vijeo Designer (all versions)

Resolution:
It is not possible to take the content from a File System Download and convert it back to a VDZ file so that modifications can be made in Vijeo Designer. The output of a File System Download is the compiled source of the project file. It is not possible to de-compile it, just like how you cannot obtain the source code from a .exe file in Windows.