Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Why ATV-IMC with Drive ILF Error.
Potential issue:
An issue is present in the park due to a bad association between the Firmware and the Hardware.
Impacted ATV-IMC date codes are between 1537 - 1606.

The bad association is:
SoMachine V3.1
Old Firmware (Firmware =< to V1.1.2.13.) – New Hardware Date code > 1536
SoMachine V4.x
Old Firmware (Firmware =< to V4.0.1.13.) – New Hardware Date code > 1536


Behaviour of the card in case of bad Association
-    The Card works without issue ( But we cannot guarantee the behaviour in the time)
-    The card is in Error immediately after Run state.
Led Err are on.
No connection possible with SoMachine.

Cards impacted:
A list of serial number is joined in order to detect easily the cards impacted. See attachment for detailed list.
This list provides:
-    The Serial Number accessible on the Card.
-    The Serial number accessible on the Box

Action recommended
-   Ask for a replacement of the card by a new one, this exchange MUST done with the information:
-"Exchange for bad Firmware association"
-In the documents associated with the return.

Schneider Electric Việt Nam

Phần đính kèm
Serial Numbers.xls [429.5 KB]
2016-06-01_1138.png [170.71 KB]