Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What to do when Web Gate says the Side-by-side configuration is incorrect?
Issue:
Web Gate is unable to launch and there is an error stating that the Side-by-Side configuration is incorrect.

Product Line:
Vijeo Designer (all versions)

Resolution:
When there is an error in Web Gate that states your Side-By-Side configuration is incorrect and the runtime cannot start, this means the Microsoft Visual Studio C++ redistributable package has not been installed properly. In order to resolve this problem, you will need to install the Pre-requisite files for the Web Gate Client files. Please contact Technical Support @ 1-888-266-8705 or customer.service@schneider-electric.com to obtain the correct version of the Microsoft Visual Studio C++ redistributable package or please find the files as attached in the zip file below.



Schneider Electric Việt Nam

Phần đính kèm
ISSetupPrerequisites.zip [6.58 MB]