Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is PME a multithreaded application?
Issue
Is PME a multithreaded application? If so, does its multiple threads run on different processors? Or, is it a single-threaded application?

Product Line
PME 8.x, 7.2.x

Environment
PME supported Windows OS.

Cause
Customer is curious to know whether PME runs on one thread or multiple threads? Is it capable of making use of multiple processors at the same time?

Resolution
PME consists of many applications. By design, they are all multi-threaded and will run across multiple processors.