Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Programming an Altivar Process Drive to communicate over Modbus Serial.
Issue:
How to set up Altivar Process Drive to communicate over Modbus Serial?

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar 600 and 900 Process Drive

Cause:
N/A

Resolution:
Basic Settings
- Programming on the Drive
  • Program Communication Settings
    • [Communication] [Comm parameters] [Modbus SL] [Modbus Fieldbus]
      • [Modbus Address] Add
      • [Bd.RateModbus] tbr
      • [Modbus Format] tFO
      • [Modbus Timeout] ttO
  • Program Command Settings:​
  • Powercycle the drive
- Communicate with the Drive
  • Using IO Profile
    • [Complete Settings] [Command and Reference] [Control Mode] - Set to IO
    • Command Word - 8501
      • Speed Reference Word - 8502 (Hz) and 8602 (rpm)
    • 16 bit word (Bit 0, 1, 2..... 15)
    • Start/Stop must turn on bit 0
      • Write a 1 to start
      • Write a 0 to stop
    • Bit 1 to 15 are assignable like logic inputs
      • Example: To assign a fault reset to bit 2 - [Fault reset] - Set to C302
  • Using CIA402 (DriveCom Profile)
    • Works with all assemblies
    • [Control Mode] CHCF to [Not separ.] SIN or [Separate]
    • Command Word - 8501
      Speed Reference Word - 8502 (Hz) and 8602 (rpm)
    • No 16 bit word
    • Start/Stop
      • Sequence of values must be written to the drive
      • 6, 7 and 15
      • Toggle between 7 and 15 to start and stop
Related FAQ: How do I troubleshoot the Altivar Process Drive when it will not connect or communicate while over a Modbus Serial Network?

Schneider Electric Việt Nam

Phần đính kèm
ATV900_Programming_Manual_EN_NHA80757_01.pdf [4.79 MB]
ATV900_Modbus_SL_Manual_EN_NHA80939_01.pdf [1.38 MB]
ATV Process MB serial 11_2014.pdf [5.01 MB]
ATV6xx_Programming_Manual_EN_EAV64318_03.pdf [5.63 MB]