Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Are the Unity Hot Fixes digitally signed.

Issue
Are the Unity Hot fixes digitally signed?

Product Line
Unity

Environment
Windows 10

Resolution
Yes, all our Unity Hotfix setup files are digitally signed.
If you right click on the hotfix and select the properties, you can see the digital signature.
sdf

All of the .exe's and dll's installed by the official release of the new Unity version 11.1 will be dgitally signed.

Cuurently, the dlls that gets installed by the hotfixes are not digitally signed.  However, ther are plans to
implement the digital signing of the dll's.