Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the minimum spacing requirement to mount an ATV660 side by side?

Issue:
Spacing requirement to mount an ATV660 side by side

Product Line:
ALTIVAR PROCESS SYSTEM

Environment:
ATV660

Cause:
Installation / Setup

Resolution:
There is no minimum spacing required when mounting ATV660, other than leaving enough room to the open the enclosure doors.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)