Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Unity Pro: Can connection modes be selected?
Issue
There is a need for logging in without the ability to make online edits, but the software defaults to programming mode.

Product line
Unity Pro, Control Expert

Resolution
Unity can be configured to prompt for connection mode so that the programmer can select what he desires. Below are definitions of the choices.

"Use Programming Mode" is the default.  It connects the terminal to the PLC
in programming mode.  If another user is logged into the PLC as the programmer,
the user is offered the option to connect in monitor mode.

"Mandatory Programming Mode".  The terminal connects to the PLC. If another user
is logged into the PLC, the connection is refused, no monitor mode offer is made.

"Use Monitoring Mode". The terminal connect to the PLC in Monitoring only mode.