Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is it possible to configure 84 circuits of a BCPM under a single device in PME?

Issue
For a 84-circuit BCPM device, customer would like to configure all 84 circuits under 1 device in PME. Drivers are done for 42-circuit BCPM, but in a case where 84 circuit BCPM is used (maximal size circuit), is there a driver available for 84 Circuits?

Product Line
BCPM, BCPM FLex Cct

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024



Environment
Device driver in Management console
Vista Diagrams of Web Application

Cause
84-circuit BCPM device - Though physically a single device, 2 BCPM devices will need to be added to PME (circuit 1 to 42 as the first BCPM device and circuit 43-84 as the second BCPM device in PME), and that is how they appear in Vista. Customer likes to see all 84 circuits under single device in Vista and Web Application.

Resolution
The current driver for BCPM and BCPM Flex Cct devices in PME do not permit displaying all 84 circuits under single device. With 84 circuits, circuit 1 to 42 and 43 to 84 have separate modbus addresses. Therefore, BCPM with 84 Circuits are treated as 2 devices (each with 42 circuits), and one BCPM device only requires 1/2 of a device license (0.5 Mid Range PME License). That is the current design of the BCPM driver. It is not possible to have a BCPM with 84 circuits as a single device in PME at the moment.