Hôm nay chúng tôi có thể giúp gì cho bạn?

[M580 HSBY]: If a value of variable stored in the primary SD card (BMXRMS004GPF) can be synchronized with the standby's?

No, the value of variable stored in the Primary SD card(BMXRMS004GPF) will not be synchronized with Standby's.