Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Uninstalling Unity Pro & going to an older version
Uninstalling Unity Pro
The following table shows how to uninstall Unity Pro manually:

StepAction
1Click Start - Program - Schneider Electric - SoCollaborative -, Unity Pro - Remove Unity Pro xx (xx refers to Unity Pro package).
2The installation wizard is launched, Unity Pro starts being removed.
3When the uninstallation of Unity Pro is completed, select the installed drivers and click Remove.
When the uninstallation of Unity Pro is completed select, in the same manner, the installed drivers, and DTMs and click Remove.

Replacing Unity Pro with a Former Version
To install a previous version of Unity Pro, the current version must be uninstalled using the Windows control panel as previously described.
In addition, the following directories must be manually removed:
  • Windows 7 (32 bits):
  • C:\Program Files\Common Files\Schneider Electric Shared\Tlb
  • C:\Program Files\Common Files\Schneider Electric Shared\Common
  • C:\Program Files\Common Files\Schneider Electric Shared\SRCSDK
  • C:\Program Files\Common Files\Schneider Electric Shared\SSTA
  • Windows 7 (64 bits):
  • C:\Program Files (x86)\Common Files\Schneider Electric Shared\Tlb
  • C:\Program Files (x86)\Common Files\Schneider Electric Shared\Common
  • C:\Program Files (x86)\Common Files\Schneider Electric Shared\SRCSDK
  • C:\Program Files (x86)\Common Files\Schneider Electric Shared\SSTA