Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What's the difference between reference XVUC9V and reference XVUC9VP?
There are following differences:
1. XVUC9V is driven by ON/OFF signal and usually connect to relay output,  XVUC9VP is driven by pulse signal and usually connect to PTO/PWM or transistor.
2. XVUC9V only supports 4 channels, XVUC9VP supports 32 channels.
3. XVUC9V supports maximum 5 layers, XVUC9VP supports maximum 4 layers.
4. For XVUC9V, the trigger signal of each channel is shared with corresponding light layer(2~5). For XVUC9VP, the trigger signal of channels is seperated with all light layers.