Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Is it possible to design a BlokSeT switchboard with some functional units with the door opening from left and some functional units with the door opening from right in same cubicle?
It is not possible to have some functional units with the door opening from left and some functional units with the door opening from right in the same column. It should be always one side opening in one column.

The hinge in BlokSeT cubicles are designed in such a way that, a single hinge assembly is used to assembly two functional unit doors(one above other). The doors cannot be completely closed because, hinge pin will interfere with door if we have two different opening.

It is not possible to assembly one left door and one right door in same column.