Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the part number of the touch-up paint for the ATV630 Outdoor drive enclosure?

Issue:
Needs the part number of the touch-up paint for the ATV630 Outdoor drive

Product Line:
ATV630


Resolution:
Schneider does not have a part number for ordering touch-up paint. Recommending acquiring the paint from Orbittx. They offer spray cans and brush bottles. Our enclosures (both wall mount and floor standing) are standard RAL7035 color.
Orbittx website:
http://www.orbittx.com/index.php?option=com_content&view=article&id=48&Itemid=53

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)