Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the cause for error 7340 on Lexium 32?

Error 7340 is triggered when the drive cannot read the absolute position of the motor's encoder.

The cause for this can be one or any of the following.

Faulty wiring from the drive to the motor encoder.

Electrical noise on the encoder signal caused by EMC.  Check for proper grounding of motor, proper grounding of motor power cable at drive and proper grounding of drive.
Do not route encoder cable near devices which create EMC.
Do not route encoder cable parallel to the motor power cable.
Do not coil excess encoder cable. Excess encoder cable should be bundled in a zig-zag pattern.

Faulty encoder within motor.
If encoder cable is not at fault and not routed near sources of electrical interference, replace motor as final step.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)