Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Where can the activation code for SoMove software be found?
Issue:
Activation code for SoMove software.

Product Line:
AC Drives, TeSys T, TeSys U

Environment:
Somove software

Resolution:
There is not an activation code for our SoMove software as SoMove is a free software. Nevertheless, you must register with Schneider Electric to be authorized to use it.
The first time you open SoMove, you will access a demo version which is only available for 4 days; you must register within these four days if you wish to continue using the software.
NOTE: Once this deadline has passed, access to SoMove access is blocked