Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
What is the PM8000's COMTRADE File Format and can it be changed?
Issue
What is the COMTRADE file name/time format, and can it be changed?

Product Line
PowerLogic PM8000 Series

Environment
COMTRADE File

Resolution
The COMTRADE files (.cfg and .dat) from a sag/swell or transient event can be found on the PM8000's FTP site.

Q: The COMTRADE file is generated with my local time, can this be changed?
A: Yes, the timestamp can be changed inside the file.

Q: Is that possible to customize the COMTRADE file name?
A: No, the file name cannot be altered (typically called cmt0__00000 (incrementing with each new saved waveform) and documented in .cfg and .dat formats).

Example of COMTRADE .cfg output:
.cfg Output
Please follow the attached COMTRADE & ION Technology document for steps on enabling the COMTRADE feature (disabled by default).
*Note: a master reset will clear all COMTRADE files on the FTP site.*

Schneider Electric Việt Nam

Phần đính kèm
COMTRADE_ION_Technology.pdf [190.42 KB]