Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Cannot connect to either a M340 or Quantum PLC with Unity 11.1 running in VMWare after updating to Unity 11.1
Issue
Unity fails to connect to the either a M340 or Qunatum PLC after updating to Unity 11.1

Product Line
Unity, M340

Environment
Unity

Resolution
Attempts to to connect to either a Quantum or M340 after updating to Unity 11.1 from Unity 11, could fail if it is installed in a VMware workstation PC..
Prior to updating to Unity 11,1 the problem did not occur.

The following can be used as a workaround.
  • Uninstall the PLCUSB Driver X64 that was installed by Unity 11.1 until a new driver is available.
fdff

  • Insert the Unity 11.0 CD
  • Open the folder named 'Communications Drivers'.
fdsf

  • Double click on the file named 'SchneiderPLCUSBDriverSuite' to install the driver.
sdfd