Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Where can you find the modbus pinout data for the VW3A3303 option card used with the ATV61 and ATV71 drives?
Issue:
Modbus pinout data location for the ATV61 VW3A3303 option card.

Product Line:
ATV61 and ATV71 with the VW3A3303 option card.

Environment:
All

Cause:
Needs the pinout data on the Sub D 9 pin connector

Resolution:
Pin 3 is DO
Pin 7 is D1
Pin 4 is Common

See attachment.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Phần đính kèm
SubD pinout for the modbus option card.pdf [46.09 KB]