Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How quiet (or noisy) is the NetShelter CX when only the fans are running, with no equipment installed?
Issue:
The question was raised asking how quiet the cabinet is with nothing installed, just the fans running.

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
Noise reduction in the office is important.

Resolution:

Noise of AR4018A / AR4018IA:
40.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet

Noise of AR4024A / AR4024IA:
43.0 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet

Noise of AR4038A / AR4838IA:
43.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet