Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Couldn't determine unit type based on ModelNum" when using EM4800 configuration tool

Issue
When connecting to EM4*** meters using the EM4800 configuration tool, an error message pops up:
"Couldn't determine unit type based on ModelNum ********-**-**"
Couldn't determine unit type based on ModelNum" when using EM4800 configuration tool

Product Line
EM4*** series meters

Environment
Meter configuration

Resolution
Uninstall the current version of EM4800 Configuration Tool that you have installed and reinstall the latest version of the tool.
The latest version of the tool from the following link:

EM4800 Configuration Tool (SEMetershop V1.6.1.1154)
​This config tool supports the new Demand feature released with meter firmware revision 1.46

* IMPORTANT NOTICE: This version is NOT measurement Canada Approved.