Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Common PowerSCADA Expert Installation/Uninstallation issues

Issue
It is possible a user can experience various errors when installing PowerSCADA Expert (PSE). See one example below:

image

"Request:RegisterAssemblies fail at function call:
RunExecutableWithReturn in broker:
BrokerFragments
\PSEProfileWizardMain.Broker.xml"


Product Line
PowerSCADA Expert 8.x

Environment
PowerSCADA Expert Installation/Uninstallation

Cause
These errors may be the result of a (previous) partial installation/uninstallation in which case remnants of PSE still exists on the machine.

Resolution
*Warning: This article contains information about editing the registry. Improper changes to the registry can permanently damage the operating system. Always backup the registry before making any changes.*

If issues are experienced when uninstalling then attempting to install a new PowerSCADA Expert version, please try the attached batch files.
Note: Run (double-click) the respective batch file of the PSE version which was previously uninstalled.

Schneider Electric Việt Nam

Phần đính kèm
Uninstall_PSE_7.40_SR1.bat.zip [1.63 KB]
Uninstall_PSE_8.0.bat.zip [1.66 KB]
Uninstall_PSE_7.40.bat.zip [1.39 KB]
Uninstall_PSE_8.0_SR1.bat.zip [1.66 KB]
Uninstall_PSE_9.0.bat.zip [1.78 KB]
Uninstall_PSE_8.2.bat.zip [1.78 KB]