Tìm các câu hỏi thường gặp
9012 G pressure switch - Snap switch in spare parts of the 9012GAWM24 pressure switch
In 2017, the snap switch in spare parts of the 9012GAW(M)24 pressure switch has part number 9998PC314, instead of 9998PC340, obsolete. Please refer to the 2009 catalogue extract, attached. Attached too the 9998PC314 datasheet.
9998PC340 & 9998PC314 are equivalent. The alone difference is the wiring diagram not included on the 9998PC314 enclosure
9998PC340 & 9998PC314 are equivalent. The alone difference is the wiring diagram not included on the 9998PC314 enclosure
Đã phát hành cho:Schneider Electric Việt Nam
Phần đính kèm
Tìm hiểu thêm
Tìm hiểu thêm