Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Do M221 controllers have retentive timers?
Issue:
Are there retentive timers for the M221?

Product Line:
TM221

Environment:
EcoStruxure Machine Expert Basic (formally SoMachine Basic)

Cause:
Programming questions on how to create a retentive timer.

Resolution:
M221 controllers have retentive timers. The checkbox for Retentive will have to be checked under the Programming tab / Tools tab / Software Objects / Timers or by clicking on the specific Timer in the program and then on the Retentive check-box.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)