Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
PME Web Report is stuck on "Report is being generated" after clicking Generate report
Issue
Customer is trying to run a report in the Web Application Report tab, and it hangs on the "Report is being generated" message. There are no errors in the system event log under Management Console, the Windows event logs, or the ApplicationModules database log files.

Product Line
Struxureware Power Monitoring 7.x (SPM 7.x)
Power Monitoring Expert 7.x (PME 7.x)
Power Monitoring Expert 8.x (PME 8.x)

Environment
Web Reports

Cause
The report logo may be missing from the default directory

Resolution
Navigate to the software install directory

For SPM 7.x:
...Program Files (x86)\Schneider Electric\ION Enterprise\web\ReportPacks\Default Reports.zip

For PME 8.0:
...\Schneider Electric\Power Monitoring Expert\web\ReportDepot\ION Reports\ION Report Packs\Default Reports

For PME 8.1:
​...\Schneider Electric\Power Monitoring Expert\config\reports

A JPEG file exists named "Report-Logo". If the file is not in the location, search to see if it is in a different location or create a new logo per FA232322.
Additionally, you can download the attached zip file, unzip the logo, and place the JPEG in the respective directory.

Schneider Electric Việt Nam

Phần đính kèm
Report-Logo.zip [51.38 KB]