Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
How do I troubleshoot an Altivar Process Drive that would not connect or communicate to a DeviceNet device or network?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Altivar Process Drive that will not connect or communicate with a DeviceNet device or network.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:

Note: This FAQ goes over some basic checks and troubleshooting tips. For extended troubleshooting please refer to your drives DeviceNet manual.

Drive Will Not Connect
  • Communication Module
    • DeviceNet is not integrated on the Altivar Process drives. Must use module VW3A3609.
    • The VW3A3609 Fieldbus module, with a minimum V1.6IE01 firmware version, is compliant with the Altivar process product range.
    • Only one communication module can be used at a time
  • Installation
  • Network
    • Check for any duplicate addresses on the network.
    • Check to make sure you have proper configured assemblies
  • Programming
    • Check Basic Settings on the drive. Make sure the following is set:
      • IP Address
      • Baud Rate
      • Data rate used
      • Make sure drive is power cycled after any Communication settings are changed.
    • Check for properly configures assemblies
  • Troubleshooting
    • Check LEDs on the drive
      • See Fieldbus Status LEDs, LED MS Network Status and LED MS Module Status  attachments
      • Drive Connects But Will Not Run
  • Network
  • Programming on the Drive
    • Confirm drive is setup for Network Control
      • Check Command and Reference Menu
        • [Complete settings] [Command and Reference]
  • ​​Troubleshooting
    • Check Communication Map
      • [Display] [Communication map]
        • ​​Check Command Channel
        • Command Register
        • Ref Freq Channel
        • Ref Freq
Reference attached manuals for further troubleshooting

Schneider Electric Việt Nam

Phần đính kèm
ATV600_DeviceNet_Manual_EN_EAV64330_01.pdf [3.47 MB]
ATV600_Programming_Manual_EN_EAV64318_04.pdf [10.52 MB]
ATV900_DeviceNet_Manual_EN_NHA80942_01.pdf [5.2 MB]
ATV900_Programming_Manual_EN_NHA80757_02.pdf [11.22 MB]
LED MS Module Status.png [217.56 KB]
Fieldbus Status LEDs.png [91.26 KB]
LED NS Network Status.png [150.18 KB]