Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
		
Hôm nay chúng tôi có thể giúp gì cho bạn?
Can other manufacturer's cabinets be installed in the HyperPod?
Issue:
Does HyperPod support other cabinet manufacturer's, or just APC NetShelter?

Product Line:
HyperPod

Environment:
All versions and serial ranges

Cause:
Customers may want to install a 3rd party cabinet into the HyperPod.

Resolution:
Yes, 3rd party cabinets can be installed in the HyperPod easily. Height differences are no problem with the adjustable brush strips that mate with the cabinet roof.